Cleaning for Health®
A Focus on the Environment and Better Indoor Air Quality
A cleaning regimen that helps dramatically reduce the levels of allergens and asthma triggers in the indoor environment.
Now more than ever, in schools, workplaces, and social places, we're thinking about the quality and safety of the air we breathe.
ProLevel Filtration® technology better captures microscopic dust that can harm health and trigger asthma or allergies. Most ProTeam vacuums have Four Levels of Filtration, each level designed to sift out smaller and smaller particles. The Intercept Micro Filter is the first line of defense.
The unique ProTeam method of suction-vacuuming cleans carpets, hard floors, and other surfaces without stirring up dust – so the air stays cleaner, the furniture collects less dust, and operators can work without breathing unhealthy air in the indoor environment.
Click the button for a 22-minute presentation by Ray Noonan, ProTeam Eastern Zone Manager on the importance of Cleaning for Health. The presentation will include: