Floors see the most intense action in a building. People spill in every imaginable area and track debris from the outdoors, especially during rough weather. For commercial cleaners, a wet/dry vac is often the best tool for the job for fast cleanups.
A wet floor can be a safety hazard, even an emergency. A multi-purpose vac can act as a lifesaver when taking care of spills and floors.
Even in worst-case scenarios, like a toilet overflow, a quick response time can mean the difference between a speedy clean-up and a full renovation. With a large capacity wet dry vacuum, you have the power and high volume to handle bigger messes.
In the construction industry, the best wet/dry vac is one with plenty of power and volume. Choosing the right tool can help keep your job site free of construction dust. And when moisture and debris make for sludge, you can rely on the powerful motor of a good wet/dry vacuum to keep things clean.
These types of vacuums are perfect for removing large volumes of dust, dirt, moisture and grime when a new construction job is complete.
When stripping hard floors, a powerful, larger capacity wet/dry vac can speed up your strip and dry process. Look for an industrial wet/dry vacuum that includes a squeegee mount to push around and recover stripping solution. An easy-to-service design makes clean out more manageable, especially when dumping your recovered stripper.
A wet/dry vacuum is also a great tool for carpet cleaning. With advanced suction and full filtration in the dry setting, a first sweep can pick up microscopic debris. Switching the vac to the wet filter setting means you can extract cleaning solution and water from wet carpets. Use an air mover to speed up the carpet drying process.
It’s important to address ergonomic pain points for big projects. In addition to powerful suction, the best wet/dry vacuum should be easy to maneuver. When choosing a wet/dry vac, look for ergonomic push handles at waist high and large wheels that swivel with ease.
Wayne Ramos has worked at a vacuum repair shop for more than 10 years. He makes the most out of his best wet/dry vac at work and home.
“I use the ProGuard 10 wet/dry vacuum. At home, I use it like I would a compact canister, cleaning in the house and out in the garage. At work, I use it when repairing other vacuums.” He also tasks it with other projects. “It works well when I use it to dry carpet faster after carpet cleaning—and to clean the water out of evaporative swamp coolers before winter.”
The applications for wet/dry vacuum cleaners are vast and should be part of every commercial cleaning crew arsenal. ProTeam® has a complete line of wet/dry vacs and air movers. To learn more, click here.