Cleaning for Health® Defined:
A cleaning regimen that helps dramatically reduce the levels of allergens and asthma triggers in the indoor environment.
Let's Clear the Air
Now more than ever, in schools, workplaces, and social places, we're thinking about the quality and safety of the air we breathe.
- According to the EPA, Americans spend approximately 90% of their time indoors
- Indoor pollutants can be 2-5 times more concentrated than outdoor pollutants
- Indoor Air Quality (IAQ) affects the health and wellbeing of building occupants
Cleaning for Health & ProLevel Filtration System
ProLevel Filtration® technology better captures microscopic dust that can harm health and trigger asthma or allergies. Most ProTeam vacuums have multiple levels of filtration, each level designed to sift out smaller and smaller particles. The Intercept Micro Filter is the first line of defense.
The unique ProTeam method of suction-vacuuming cleans carpets, hard floors, and other surfaces without stirring up dust – so the air stays cleaner, the furniture collects less dust, and operators can work without breathing unhealthy air in the indoor environment.
Cleaning for Health® Webinar
Click the button for a 22-minute presentation by Ray Noonan, ProTeam Eastern Zone Manager on the importance of Cleaning for Health. The presentation will include:
- What is the difference between cleaning for appearance and Cleaning for Health
- Why high-performance cleaning is important to improve IAQ
- How cleaning pros can clean for health with optimum efficiency
American Lung Association
ProTeam is a proud partner of the American Lung Association. Together, we fight for clean indoor air so that we all can breathe easier.
For more information on indoor air quality, call 1-800-LUNG-USA or visit Lung.org. The American Lung Association does not endorse product, device or service.