From Floor to Ceiling:

Cleaning for Health Made More Productive with ProTeam GoHigh™ Dusting Kits

Clean floors are an important part of facility maintenance, but they’re only part of the high interior dusting picture. Dust and debris can accumulate well above eye level on vents, ductwork, ledges, light fixtures, high ceilings, and overhead beams. Left untouched, these hard-to-reach surfaces can become reservoirs for dust and allergens that may become airborne and contribute to poor indoor air quality.

For cleaning professionals, the challenge is reaching those surfaces without sacrificing productivity or adding unnecessary complexity to the cleaning routine. High dusting may require ladders, lift equipment, additional setup, or even another team to handle the work. ProTeam GoHigh Dusting Kits offer a more efficient approach by extending the reach of compatible ProTeam corded backpack vacuums, helping crews tackle elevated surfaces while keeping their feet on the ground.

What Is Indoor Air Quality?

The EPA defines indoor air quality (IAQ) as the quality of air within and around buildings and structures and its impact on occupant health, comfort, and well-being. For cleaning professionals, supporting IAQ starts with managing contaminants that accumulate throughout a facility. Dust, allergens, and other particles can settle on floors as well as vents, lighting, ledges, ceiling fans, and other elevated surfaces—and can become airborne again when disturbed by airflow, activity, or routine maintenance.

That’s why effective cleaning is about more than making surfaces look clean. It’s about capturing, containing, and removing contaminants at the source. ProTeam vacuums combine powerful suction with ProLevel Filtration®, which is 99.9% effective at capturing and containing particles 1 micron and larger from surfaces. GoHigh Dusting Kits extend that cleaning capability upward, helping crews capture overhead dust and allergens while supporting a more complete approach to Cleaning for Health.

Productivity: Clean More in Less Time

High dusting can be difficult to fit into an efficient cleaning workflow. Setting up ladders or lifts, moving equipment into position, and coordinating additional resources can turn what should be a routine task into a separate operation. GoHigh Dusting Kits help crews clean more in less time by extending the capabilities of the ProTeam corded backpack vacuum they already use. The pole system uses a simple push-button locking design, making it easy to assemble and adjust the reach for different cleaning tasks. Crews can transition from floor-level cleaning to elevated surfaces without setting up a lift or significantly interrupting their workflow.

Available in Standard and Max configurations, GoHigh provides 13 feet of additional reach with the Standard Kit and 26 feet of additional reach with the Max Kit. Both kits come with a modular design that allows crews to adjust the number of poles based on the task. That flexibility allows teams to incorporate high dusting into routine cleaning rather than treating it as a separate job requiring additional equipment or resources.

The system also gives crews the tools to tackle different surfaces without changing equipment or introducing another step to the workflow. The pipe tool helps clean round surfaces such as pipes, vents, and ductwork, while the round dust brush is suited for fixtures, ledges, decorative lighting, fans, and shelves. For broader horizontal surfaces, the ProBlade® helps remove dust from areas that can otherwise be difficult to reach. 

With the reach, tools, and flexibility to handle multiple applications, GoHigh Dusting Kits help make high dusting part of the regular cleaning workflow.

Safety: Take the Risk Out of Ladders and Lifts

Working at height can introduce additional risks when cleaning requires ladders or lift equipment. GoHigh Dusting Kits provide an alternative for many routine high dusting applications by allowing cleaning professionals to work from the ground. The extended reach of the GoHigh system allows crews to clean elevated surfaces without climbing. Keeping cleaning professionals on the ground can help reduce the risks associated with ladders and lifts while making high dusting easier to incorporate into routine maintenance.

Ergonomics: Reach Higher Without the Extra Weight

High dusting can also place physical demands on cleaning professionals, particularly when tools are held overhead for extended periods. GoHigh Dusting Kits are designed to provide extended reach without adding unnecessary weight to the task.

The carbon fiber poles are nearly half the weight of aluminum while providing approximately twice the strength, enabling people of all heights to use the kit while maintaining control and maneuverability when cleaning overhead. The lightweight construction helps reduce the physical strain of reaching elevated surfaces, while ground-level operation eliminates the need to repeatedly climb, reposition, and descend ladders during the task.

GoHigh also includes specialized tools and angled bends to help operators approach different surfaces without excessive reaching or awkward positioning. The 45° and 135° bends, along with the optional 90° bend, provide flexibility for accessing areas around obstacles, overhead ledges, and elevated horizontal surfaces.

Total Cost of Ownership (TCO): Invest Once, Reach Again

High dusting doesn’t happen just once. Facilities need to maintain elevated surfaces as part of ongoing commercial cleaning programs, and relying on lift rentals can add recurring costs and complexity. Aerial lift rentals can range from roughly $125 to $500 per day or $375 to $1,500 per week, before factoring in delivery, pickup, training, operators, and crew time spent repositioning equipment. For quarterly high dusting, that can add up to roughly $1,600 to $2,000 each year.

GoHigh provides a reusable alternative that attaches to the compatible ProTeam corded backpack vacuum you already own, eliminating the need for a second machine. At approximately $1,700 list for the Standard Kit and $3,050 list for the Max Kit, the kits can pay for themselves in roughly one to two years of quarterly lift rentals. After that, high dusting can shift from a recurring rental expense to an in-house cleaning task.

This can be especially valuable during school summer breaks, when teams have a limited window to complete deep cleaning before the next school year. Without a lift to schedule, deliver, set up, and reposition, crews can spend more of that limited time cleaning. Invest once in a GoHigh Dusting Kit and reach again—without the recurring cost and coordination of lift rentals.


Ready to take commercial high dusting to the next level?

Learn more about GoHigh Dusting Kits